STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F745ZG ethernet high payload transmission problem

Hi,I have been trying to implement a TCP server on a STM32F745ZG MCU using lwip library and ST example codes, however while I am trying to send data packets with payload bigger than 1460 bytes, my server wont be able to replay the client packet and t...

Screenshot 2024-05-23 112650.png
amirshn by Associate III
  • 5172 Views
  • 9 replies
  • 3 kudos

STM32H573I-DK_aws_ri_tz certificate

I'm working with the stm32h573i-dk kit and I need a connection to AWS. I performed the step-by-step procedure as described in the webinar https://content.st.com/stm32h5-connects-smart-things-in-a-secure-way.html, however, I got stuck at the end, wher...

ffjunq_2-1712689414514.png
ffjunq by Associate III
  • 3871 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F303VC clock setup with crystal on OSC_IN

We have custom HW with an STM32F303VC processor.There is a 12 MHz crystal with an 18pF in parallel wired to OSC_IN and OSC_OUT.The power budget is basically unlimited so we would like to run the device as fast as possible with this configuration.Peri...

jlag_0-1716560475207.png jlag_2-1716560572625.png
jlag by Associate III
  • 1424 Views
  • 1 replies
  • 1 kudos

STM32F4 Timer Counter Never Starts Counting

Hi, I am attempting to enable TIM1 to act as my program's tick timebase as SysTick is being utilized by the FreeRTOS kernel to generate PendSV interrupts. I configured this in CubeMX (Timebase set to TIM1) but I cannot get TIM1 to start ticking. Atta...

notTicking.png
Elliott99 by Associate II
  • 2190 Views
  • 4 replies
  • 0 kudos

SerialPort with registers

Hello, I am trying to do one simple task with my STM32 board using just registers and interruptions in USART2.Basically I have to wait until I receive data via serialPort, then activate interruption that should increment the value of my data by 1. Af...

summ98 by Associate
  • 830 Views
  • 1 replies
  • 0 kudos

STM32F4 Timer DMA requests

Hello Team,I am using the STM32F469NIH6 to implement a timer triggered DMA and I need some clarity on a few points here-I see that that there are three possible requests possible for a timer triggered DMA. I understand that the TIM8_UP is to trigger ...

Jansunil_0-1716460451673.png
Jansunil by Associate II
  • 3236 Views
  • 5 replies
  • 0 kudos

Resolved! Program won't run after upload

I have designed my own PCB and I have the problem that while the code uploads successfully, it doesn't run.I have checked NRST and BOOT0 and both should not be the problem. I have found a similar issue where the chip didn't get a clock signal and the...

Qwyntex_0-1716384046463.png
Qwyntex by Associate III
  • 12085 Views
  • 22 replies
  • 3 kudos