User Activity

Hello,For my project I am working on two nucleo board H743ZI2.Unfortunately, during an experimentation one of the boards ceased working (LD4 and LD6 red). Maybe a short circuit, I don't know.Anyway I tried to purchase a new NUCLEO-H743ZI2 but it seem...
Hello,The main purpose of the question is to avoid giving source code and give binary file instead.For example, I generate a compiled binary file from a nucleo project (STM32H743ZI2) for the M7 core.Then I want to create a new dual core project (STM3...
Hello, I am using a nucleoH743ZI2 and STM32CubeIDE v1.13.2 on windows10I configured the USART 3 in order to receive some telecommands from my laptop (windows 10) using a software (HTerm v0.8.9)The telecommands are written in binary, 52 bytes, but the...
Hello,I am using a NUCLEO-H743ZI2 and program on the STM32CubeIDE1.13.2The purpose of my project is to create a 2kHz sine and to sample it at 40kHz at the same time.I would like to have no delay between the 12bits DAC and the 12bits ADC: that the fir...
Hello,I am using a NUCLEO-H743ZI2.I read the reference manual RM0433 Rev8.I also read a bunch of topics in the forum but didn't find what I wanted. I am trying to check my ADC sampling rate by looking at the timestamp at my half full/full callback fr...
Kudos from
Kudos given to