Hi Madam/Sir,I have flashed the firmware of STEVAL-IDP004V2 to my own version, now i want to flash back, where can I download the default firmware when I bought it?thanks
How to open the STSW-IO-LINK evaluation firmware in the STM32CubeMX development platform? STSW-IO-Link is downloaded and extracted. The *.ioc file seems to be missing in the STSW-IO-LINK firmware package!
ok, here are 2 more questions.1. may I know which develop environment used to develop STSW-IO-LINK firmware if it is not CubeMX?2. the default firmware in STEVAL-IDP004V2 is STSW-IO-LINK or not?thanks.
thanks for your information. if I want to change the firmware code and download it to MCU, do i need to start from 0 to create my own project and code? or do I have any other ways more easier?