User Activity

Hello,I am reading AN2606 and I am wondering if I am interpreting the document correctly. Is table 113 suggesting that the FDCAN bootloader is only available on pins PH13 & PH14 in the STM32H75 series? Since these pins do not exist on the 100 pin pac...
Per section 2.6 of RM0433 (https://www.st.com/resource/en/reference_manual/rm0433-stm32h742-stm32h743753-and-stm32h750-value-line-advanced-armbased-32bit-mcus-stmicroelectronics.pdf), when the STM32H7 boots up it latches the boot pin and then goes to...
Section 6.4.4 of RM0433 is the only place I could find that says what to do with VBAT rail when not using a battery. It says the following:If no external battery is used in the application, it is recommended to connect VBAT externally to VDD through ...
Kudos from
Kudos given to