STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H723 I2S or SAI

Hi,I need to use the I2S (or SAI) interface to connect a codec stereo working at 48KHz, 32bit word length and I2S connection; when I configure the multimedia I can select the SAI interface (SAI1 or SAI4) or one of the I2S interface available.Which ar...

carloV by Associate III
  • 4639 Views
  • 2 replies
  • 0 kudos

bootloader on usart1 not working on stm32h747

hi,i have a custom board with stm32h747xih6. i am trying to boot the device from usart1 on pins PA9/PA10 with no success. booting from usart1 on pins PB14/PB15 is working fine but requires new layout. jtag works fine too.when trying boot from PA9/PA1...

PShad.2 by Associate
  • 1913 Views
  • 2 replies
  • 0 kudos

Resolved! Understanding uSD and MCU changing

Hi, I was trying to have microSD logging with F439 Nucleo. I can't see example with mentioned board. Please let me know:1. example for mentioned board to log data in microSD2. I tried configuring SD-4 bit, but couldn't identify the pins intialized in...

GauravK by Senior
  • 5269 Views
  • 13 replies
  • 3 kudos

Resolved! UART FIFO depth

Hello good day,I am using the STM32H755 Nucleo board. In the UART module, how are the FIFOs managed? According to the datasheet, there is one TX FIFO and one RX FIFO.What is the actual depth of these FIFO?

sarun by Associate III
  • 2758 Views
  • 3 replies
  • 1 kudos

problem in generating hse

we are using UFBGA 132 for BLDC motor control with HSI clock to reduce the power consumption, we have been trying out with HSE clock by enabling PD10 to high, hereby, if we try to debug it get struck in the error handler function and the status of th...

Resolved! MBED TLS and TCP

Hi ,I need to use MBED TLS and TCP in F429ZI board. I didn't see any example codes for the same . Can anyone Please share the example code.