STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB PD in STM32L562

Hi Team, I need to build USB PD program on ST32L562, The voltage they are expecting is up to 45V. How to do this?RegardsNithin

NITHIN by Associate III
  • 2910 Views
  • 7 replies
  • 0 kudos

SPI communication

I used STM32F407VGT6, software-driven SPI, and analyzed with a logic analyzer, and the unpacking corresponded to the program, but there is no signal for this module, that is, it has a problem

STM32L1 HardFault after wakeup from sleep mode + fix

I would like to share a bug I encountered and how to fix it:I am using an STM32L151, the goal is to set it into SLEEP mode and wake it up using a UART receive interrupt while debugging. All configurations to pins, registers and interrupts are made co...

makas005 by Associate II
  • 3897 Views
  • 5 replies
  • 2 kudos

Resolved! CAN-bus with STM32F103RB

Hello there!I am trying to use some STM32F103RB Nucleoboards and some MCP2551 chips to make a CAN-bus. I got this problem where I can make it work in loop-back mode, but I cannot send from one board, to another one. I know the Circuit is stable and c...

Kenno by Associate II
  • 3596 Views
  • 1 replies
  • 0 kudos

Resolved! USART4 Tx idle stays low STM32G070

Hello everyone,I successfully used USART1 and USART3 in my application. However, when trying to use USART4, Rx is working but not Tx. The idle signal stays at 0V all the time. Here is what I already check:UART initstatic void MX_USART4_UART_Init(void...

PSicl.2 by Associate II
  • 6824 Views
  • 11 replies
  • 1 kudos