User Activity

Hi all,I'm having problem implementing a function to change the baudrate during runtime. I've read all the other topics about it and tried the proposed solutions but couldn't get it to work, maybe I missed something.I use DMA for the UART which might...
Hi all,I am trying to launch the app from a bootloader code that I copied from a project on an STM32L0 and STM32F446, it worked fine there but somehow my app doesn't start on the STM32G491.Here's the code for the jump:  static void bootloader_jump_to...
Hello,I'm having problems with the adc conversions on my STM32G491.There is an error of 23-26% higher than measured with scope or multimeter.I'm using ADC1 & 2 in dual mode with DMA, I have an input signal coming from an opamp voltage follower.I'll a...
Hi all,just found an error preventing the adc from working properly when the driver is generated by STM32Cube FW_G4 V1.5.2 (and 1.5.1).there are some missing lines like this one:sConfig.Channel = ADC_CHANNEL_2; you can compare my 2 attached files to ...
Posted on June 07, 2018 at 12:16Hello,I am using the code supplied by ST for the X-NUCLEO-NFC05A1, with a different processor (STM32L031) than on the demo NUCLEO board, to control the ST25R3911 with ISO15693.This code comes from the example STM32Cub...