STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Program update

Hi,1. is there any tool (GUI) to update program using executable?2. How to have different modes of programming? (UART/ USB/ sd card)3. Bootloader mentions: USB OTG FS (PA11/12) in Device mode (DFU: device firmware upgrade). Can external HS phy in FS ...

GauravK by Senior
  • 6087 Views
  • 16 replies
  • 1 kudos

STm32h735 Display change

Hello, I am doing a project on making a car display using STM32H735, but the Display on it is small, as you know, for the cars. so, is there any way I can use another LED screen for the display on which I put all the data from my STM32H735 board and ...

JM4 by Associate II
  • 775 Views
  • 0 replies
  • 0 kudos

STM32H745-DISCO SPI problems

Hey everyone,I have issues with my SPI2 on STM32h745 DISCOI am Using SPI2 to connect an accelerometer to my board. I use this SPI because it is the one that is connected to my arduino pin. SPI initialization : static void MX_SPI2_Init(void) { /* U...

fru99999_0-1717491877238.png fru99999_1-1717491895632.png fru99999_2-1717491931454.png fru99999_3-1717491956603.png
fru99999 by Associate
  • 1660 Views
  • 2 replies
  • 0 kudos

Resolved! ADC Polling Returns Same Value for Each Sample

There are four DC fans connected the board.  For each, there is a current resistor buffered through an op-amp and then passed to the ADC channel on the STM32G491RET6 MCU. All four ADCs are connected to the same module on four different channels. Soft...

DRad by Associate
  • 1957 Views
  • 2 replies
  • 0 kudos

Resolved! ADC DMA/programmed start/stop by timer compare?

Hallo Gurus:Newbie level question..'health issues' making me less efficient, and some pointers to get me started would help a lot.I want to do a software start of ADC conversions with DMA into a circular buffer...when an external trigger (GPIO?) occu...

Lohi by Associate III
  • 1815 Views
  • 2 replies
  • 1 kudos