2024-02-01 8:44 PM - last edited on 2024-04-01 8:06 AM by mƎALLEm
Hi Everyone,
I'm facing the issue that when i implementing the CAN interrrupt Transmit(CAN_IT_TX_MAILBOX_EMPTY) in CAN Normal mode. It going to interrupt hardfault error. But when i'm using the same concept in the loopback mode. It is working fine. so can you please provide the reason.
2024-04-01 8:00 AM
Hello,
You need to provide more details.
If possible to share your project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.