STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H730 outside of program code

Hello!I'm porting a working code from H750VB to H730VB, generating a new HAL core from STM32CubeMX, but right after entering on "SystemClock_Config" function at debug mode, I've got the message "Break at address 0x46bd3718 with no debug information a...

Peaga by Senior
  • 9018 Views
  • 18 replies
  • 9 kudos

Resolved! STm32CubeMX bug: CAN2 wrong configuration

Posted on June 26, 2014 at 16:31 Hi, I tried to configure my STm32F207 using the ''Cube'' to use the CAN2 and I found a bug. This is the initialization code generated by the ''Cube'': void HAL_CAN_MspInit(CAN_HandleTypeDef* ...

Resolved! Same project, two different ioc files

I have a working project with its .ioc file.Now I need to port the project codebase to another project that uses exactly the same processor, but with different pinout: the peripherals in the project will be the same, mapped on some other pins.I need ...

Resolved! Cannot uncheck "save power of non-active UCPD" in ioc

Hey All, I cannot seem to uncheck the option "save power of non-active UCPD - deactive Dead Battery pull-up" Everytime I generate code I have to manually comment out (disable) (HAL_SYSCFG_StrobeDBattpinsConfig(SYSCFG_CFGR1_UCPD1_STROBE | SYSCFG_CFGR1...

Screenshot 2024-04-01 091533.png
s_bhonwal by Associate II
  • 2602 Views
  • 2 replies
  • 0 kudos

STMG0 Multichannel ADC CubeIDE configuration issue

Hi,I'm not able to set the STM32G030C6 ADC1 for 9 + Internal Temperature Sensor channels. Here's my ADC1 Mode and Configuration parameters I'm using this recently updated Software Package VersionSTM32CubeG0 Firmware Package V1.6.2Does anyone know wha...

Gaston_1-1719938564685.png Gaston_2-1719938744194.png
Gaston by Senior
  • 2080 Views
  • 3 replies
  • 0 kudos

Sampling frequency issue

Hello,I am using an STM32U585CIU6 with LSM6DSOX to sample acceleration values, in order to use it in a project on NanoEdge. I am facing an issue while trying to sample higher frequencies. My accelerometer is set to operate at 833Hz. By printing the n...

STM32 NUCLEO-H743ZI2 UART Baud rate mismatch problem

Currently i am working with nucleo-h743zi2 board. I set the Baud rate in CubeMx to 115200. In the Hercules program, when I set the baud rate to 115200, the data does not flow correctly, but when I set the baud rate to 38400, it flows correctly. Why m...

uart.PNG
Chaotic by Associate II
  • 3851 Views
  • 7 replies
  • 2 kudos