Question
Updating firmware via IO-Link
Hello,
I have a question regarding doing a firmware update via the USART-pins and IO-Link.
Would it be possible to use a IO-link master module to sent an update to the L6362A which translates it to 3.3V UART for the STM32G0B1KEU6 we are using in our current project.
I couldn't find anything about this. It seems possible but I would need some guidance.
We're using the UART1_pins. These allow for a firmware update on them.
Thanks in advance!