STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reading two PWM signals using only two channels.

Hi! Library used: Standard Peripheral Library (Yea, I must use this one)Hardware:Test bench that can generate two pwm signals ( A and B )Cable that connects the test bench to the other boardOther board that should read the signal, delivered by the ca...

Resolved! STM32 H5 I3C 0x7E start byte in I2C waveform

Hello,I am trying to use the I3C interface between STM32H563ZI in MB1404 board and NXP's temperature sensor P3T1085UK. I have found a question would like to be answered: Is there any way to send the IBI header (7'h7E) with SCL signal configured in I2...

spike_filter.png IBI_header.png
Ren1 by Associate
  • 2517 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F030 Halts upon enabling ADC

Hi,I am new to STM32 MCUs and working on a small project at the moment. I following the reference manual but facing an issue that as soon as I enable ADC in CR, the MCU stops responding. I have attached the following code if someone could guide on wh...

x4ce by Associate III
  • 1199 Views
  • 1 replies
  • 0 kudos

Issue with Running Application from Bootloader

I seek your assistance with an issue I'm encountering while attempting to jump from my bootloader to an application stored at a specific address in the flash memory of an STM32H723ZGT6TR microcontroller.  I am able to successfully flash the applicati...

STM32 Timer PWM mode, strange behaviour

Hello!I am using a STM32F303 MCU. I am generating a complementary PWM signal with a dead time. During operation I am changing the dutycycle of the PWM. I noticed a very strange behaviour. As soon as the counter value reaches the compare value, the ou...

Resolved! HAL - Interupt-driven I2C, USART

Hi,I am new to the STM32 world and currently working on the following application on a STM32F103CBT6 @72MHz:1. Collect data from I2C sensor triggered from external interrupt @800Hz2. Read commands (MODBUS RTU) from USART and respond.I set up the uC w...

darkridge by Associate II
  • 3563 Views
  • 5 replies
  • 0 kudos