STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Measure frequency of many lines

Hello, I'm developing a board to control a desk pc setup.In addition to other things like controlling the lights, some motors and other stuff, the board has to control and monitor some PWM fans.The fans report back the revolutions using a tachometer,...

BRapo.1 by Associate II
  • 1259 Views
  • 1 replies
  • 0 kudos

Jump to Boot app

Hello, I am using bootloader software on stm32U5 microcontroller. After updating the software while in boot mode, the processor jumps to the user app without resetting itself. However, when jumping from the User app to the boot app, it does not switc...

cetin by Associate
  • 1260 Views
  • 1 replies
  • 1 kudos

STM32f446re

HAL_ADC_Start(&hadc1); HAL_ADC_PollForConversion(&hadc1,1000); readValue1 = HAL_ADC_GetValue(&hadc1); HAL_ADC_Stop(&hadc1); HAL_Delay(100);   HAL_ADC_Start(&hadc2); HAL_ADC_PollForConversion(&hadc2,1000); readValue2 = HAL_ADC_GetValue(&hadc2); HAL_...

Reading two PWM signals using only two channels.

Hi! Library used: Standard Peripheral Library (Yea, I must use this one)Hardware:Test bench that can generate two pwm signals ( A and B )Cable that connects the test bench to the other boardOther board that should read the signal, delivered by the ca...

Resolved! STM32 H5 I3C 0x7E start byte in I2C waveform

Hello,I am trying to use the I3C interface between STM32H563ZI in MB1404 board and NXP's temperature sensor P3T1085UK. I have found a question would like to be answered: Is there any way to send the IBI header (7'h7E) with SCL signal configured in I2...

spike_filter.png IBI_header.png
Ren1 by Associate
  • 2505 Views
  • 1 replies
  • 0 kudos