cancel
Showing results for 
Search instead for 
Did you mean: 

Please guide me

CG3
Associate III

I have stm32 board :

 

NUCLEO-L496ZG-P

 
and would like to make a simple helo word code in C and see out put by SWD debug connector in ITM unit (FIFO), 
 
SO i create simple hello word as follow:
IDE : stm32cubeide
New > stm32 project > chose above board , 
main.c :
#include<stdio.h>
#include <stdint.h>
and 
int main(void)
{
printf("Hello World\n");
    /* Loop forever */
for(;;);
}
 
then add this code to syscalls.c as i found in internet :

/////////////////////////////////////////////////////////////////////////////////////////////////////////
// Implementation of printf like feature using ARM Cortex M3/M4/ ITM functionality
// This function will not work for ARM Cortex M0/M0+
// If you are using Cortex M0, then you can use semihosting feature of openOCD
/////////////////////////////////////////////////////////////////////////////////////////////////////////


//Debug Exception and Monitor Control Register base address
#define DEMCR         *((volatile uint32_t*) 0xE000EDFCU )

/* ITM register addresses */
#define ITM_STIMULUS_PORT0   *((volatile uint32_t*) 0xE0000000 )
#define ITM_TRACE_EN           *((volatile uint32_t*) 0xE0000E00 )

void ITM_SendChar(uint8_t ch)
{

//Enable TRCENA
DEMCR |= ( 1 << 24);

//enable stimulus port 0
ITM_TRACE_EN |= ( 1 << 0);

// read FIFO status in bit [0]:
while(!(ITM_STIMULUS_PORT0 & 1));

//Write to ITM stimulus port0
ITM_STIMULUS_PORT0 = ch;
}

build and it work good, 
 
connect board by mini usb to PC USB
and as I check window , it connect and working
 
finally try to debug but IDE give error message : 
 
No ST-Link detected , Please connect ST-link and restart the debug session,
Please recommend if i miss some point ?
 
thank you in advance
 
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @CG3 

Could you please try using an other USB port on your PC and ensure that you are using a USB data cable and not a charging cable. Finally, don't forget to check that all the steps of the part 3.1 of the UM2179 are verified.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.