STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 Possible to disable CAN bootloader?

I have a product that contains 2 STM32F405/07/15/17 series MCUs. There are 2 because we need 4 CAN and that's cheaper and easier than finding a 4 CAN MCU. Anyways, the main MCU is connected to the secondary MCU via UART and the boot/reset pins so tha...

LLawr.1 by Associate II
  • 1604 Views
  • 2 replies
  • 0 kudos

STM32H7 ECC IRQ

I am trying to understand how the ECC IRQs work.  I have configure the RAMECC1 AXI SRAM, RAMECC2 SRAM1, 2 and 3, and RAMECC3 SRAM 4 monitor CR registers to generate interrupts on double bit errors.  I have configured the IER so that Global interrupts...

NBrick67 by Associate II
  • 1151 Views
  • 1 replies
  • 0 kudos

Resolved! ISR function timing period issue

Hi        We are working on STM32H503 MCU which has ARM Cortex 33. In datasheet it is provided that 12 cycles or instruction to enter into an interrupt function. Configured system clock as 250MHz, with that we could reach an interrupt function within...

I2C slave does not Ack when not in Debugging mode

I am trying to make an I2C slave that returns a fixed number of bytes to master upon being called with a read from the master (7Addr-Bits+1Read-Bit). In Debug-Mode it works, in normal run, it doesn't.I have thrown almost any HAL-functionality out, an...

Resolved! FMC: Data integrity in SDRAM

Hi everyone,I am observing some data corruption in an external SDRAM connected to an STM32 F7 FMC peripheral and I am trying to understand what is happening and how to prevent it. Scenario:Configure the FMC to interface with a Winbond external SDRAM ...

BrMel10_1-1721299239655.png
BrMel10 by Associate II
  • 4321 Views
  • 8 replies
  • 3 kudos

Resolved! Problem with IWDG and WWDG timeout

Hello ST Community and Support Team, I try to play with Independant Watchdog and Window Watchdog on a Nucleo U575ZI eval board.I was able to configure counters, window and even EWI interrupt perfectly thanks to STM32 HAL library watchdog related func...

Resolved! STM32H563 EDATA Size - Code Generation Issue

Hello,I am using the Cube Code Generator, within the STM32CubeIDE (version 1.13.1) for an STM32H563, and have configured the Flash Data Sectors to use the maximum 8 sectors per bank for EDATA. The valid range for the EDATA sector size is 0 - 7, as sh...

lpfeiffer_0-1699395038922.png