User Activity

Hello everyone,I'm designing a new system based on the STM32F746BET6.Basically it's just reading and writing GPIOs and receiving/transmitting data through a few interfaces (ethernet and I2C). The system receives a 100 bit/sec data frame every second ...
Hello everyoneI'll receive soon a custom board based on an STM32 microcontroller (still not sure about the specific part number) and I'll have to flash FW updates on it. A few questions about it:1) There's a 4 pin header connector on the board (VCC, ...
Hello everyone.I'm interfacing my STM32F745IET6 (master) with an SPI device.I'm using SPI1 interface running at 50 MHz, I was wondering if there's some "rule of thumb" to calculate time needed (in terms of clock cycles) to write n bits over the bus. ...
Hello everyoneIs it possible to program my STM32F745 via RS-485 using the integrated bootloader?My idea is using USART1 (as written in the AN2606) and a transceiver to do that. Has anyone done something similar? Thank you very much in advanced. Best ...
Hello everyone,I want to use the MT46V64M8P-5B:J 64Mx8 SDRAM by Micron with a STM32F745IET6 microcontroller.I'm configuring the peripheral on stm32IDE and it looks fine, the configurator automatically set PG8 as clock signal. Still, the SDRAM require...
Kudos from
Kudos given to