cancel
Showing results for 
Search instead for 
Did you mean: 

stm芯片程序跑死机

西安汇越
Associate
测试故障如下:
1. 故障现象:不上数据,不能进入网页; 测试步骤:1.拆回设备2.通过网络连接网络拾音器网络1,能ping通,进入不了网页。连接网络拾音器网络2.能ping通,能进入网页,设置完IP准备连接服务器,发现网页有连接不上了4.通过串口看,发现程序没有跑起来。通过反复上电,发现程序每次跑的结果不一样,有时一上电就死机,有怀时能跑几士秒5.好、坏板子互换芯片(stm32),坏板子更换序号为0x42-0x00-0x35-0x01-0x57-0x46的芯片,工作24小时一直正常。好板子更换0x26-0x00-0x2B-0x01-0x57-0x46的芯片,故障依旧。
2.故障现象:上数据,数据大小不一;测试步骤:1.拆开设备连接串口检测。2.一连上服务器,程序就会重启,不连服务器不会重启3.用示波器测量电源会在发送网络数据是出现约0.5v的毛刺,同时设备重启,好板子却无该现象。4.更换序号为0x42-0x00-0x35-0x01-0x57-0x46的芯片(stm32),目前工作4小时无问题。而和它互换芯片的板子故障重现
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STOne-32
ST Employee

Dear @西安汇越 ,

Welcome in our Community. To better assist you may be you can give more details on the exact product number and more information on the issue , you can post it here and my colleagues in Our Chinese Community will help you : https://shequ.stmicroelectronics.cn/

 

谢谢

STOne-32