STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB PD Dead Battery Issue

My STM32H533VE works as PD Sink.We connected CC1/CC2 with DBCC1/DBCC2 (as AN5225), STM32 cannot power up with a USB PD adapter. The adapter supplies power for ~20ms then stops the supplying.If I remove the long time initialization code (LSE initializ...

xufl by Associate II
  • 455 Views
  • 3 replies
  • 0 kudos

STM32H750 and USB3300-EZK has stopped working

I designed a board that uses a STM32H750 with a USB3300-EZK that has stopped communicating over USB. It's been having intermittent issues for the last day or so (sometimes I'd need to power cycle the board before it would show up, but then it would w...

sophie by Associate II
  • 626 Views
  • 10 replies
  • 2 kudos

Resolved! STM32H573 PB14

In our project I use STM32H573VIT6 LDO uC. We have a problem with the PB14 pin. We use 3 pins for LED control (PB10, PB13 and PB14, see photo). The problem with the PB14 is that the LED lights up dimly without code initialization. If PB14 is initiali...

gaso111 by Associate II
  • 14395 Views
  • 27 replies
  • 11 kudos

800 x 800 Display with STM32U5G9VJT6Q - possible?

Hi,we are trying to get a 800x800 display to work with the STM32U5G9VJT6Q, using either RGB888 or RGB565 in Video Mode (Burst).According to what we read it is definitely possible. Did we miss something?Could someone please confirm that is definitely ...

Ricko by Senior III
  • 7219 Views
  • 32 replies
  • 16 kudos