User Activity

Hi All, I have a STM32 Nucleo H723ZG development board and running CMSIS RTOS v2 and HTTP server with netconn  on it. The project is an example provided by the ST and it is available in STCubeMX. everything works fine until I disconnect the Ethernet ...
Hi all, Is there a Modbus tcp/ip Server (Slave) and client (Master) examples for STM32 Nucleo F429ZI board or any other similar boards?  Thanks,
Hello everyone,  I have been trying to run a simple LWIP application on my STM32 F429ZI board. I can see the LED green and orange of the Ethernet jack (CN14) are on which indicates the link is up and running. but no luck with pinging the board from m...
Kudos given to