STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

print messages are not coming in teraterm

Hai,I am using STM32L496ZG-P board and STM32CUBE IDE (1.15.1). I tried to print hello world in tera term using UART/USART,USB etc , i tried many programs by reffering many videos in youtube, and some docs from STM communinty link etc etc,. Maximum al...

Resolved! USB_DEVICE code can't work!

Hi there,I am using STM32F429BIT6 and want to show the SDcard(connect with MCU by SDIO) as a Udisk on PC.I can normally read/write the SD card by MCU with FATFS.But after I added the USB config in CubeMx, the code is something wrong.My CubeMX config ...

Junde_0-1723691539237.png Junde_1-1723691568096.png Junde_2-1723691618953.png Junde_3-1723691695548.png
Junde by Senior III
  • 1685 Views
  • 2 replies
  • 1 kudos

Resolved! HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY) fails in HAL_MspInit.

Hello,I am currently working with the STM32H7R7I8T6 and I am having issues configuring the Power. When HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY) is called in the HAL_MspInit function, it fails waiting for the PWR_SR1_ACTVOSRDY bit to set. I have measure...

Screenshot 2024-08-11 at 3.21.17 AM.png
Kwame by Associate II
  • 3013 Views
  • 4 replies
  • 0 kudos

Resolved! NUCLEO-G474RE Arduino

Hello everyone, I'm new here, I want to start like this first. Today I bought the NUCLEO-G474RE card. I will use this card in a battery management system. My previous system was DC2026C+DC2792B(LTC6820)+DC2350B(LTC6813), this way I can read voltages ...

khalih by Associate
  • 1967 Views
  • 2 replies
  • 2 kudos

Running STM32H725 SPI at higher frequencies

I'm working on my first STM32 project and have an stm32h725rg configured as a SPI master. Ideally, I'm aiming for a clock frequency of 60 MHz but had to slow it down to 12 MHz (the lowest that my sensor can be configured for) after an initial round o...

llee__2-1724259080750.png
llee_ by Associate
  • 3504 Views
  • 5 replies
  • 1 kudos