STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Read 3 analog signals; 5 - 20 kHz sampling rate

Hello,I have two core boards:1st: Nucleo-64 with STM32L476RGT6U 64 pins, 1Mb of flash memory and 128 Kbytes of SRAM.2nd: Nucleo-144 with STM32F429ZIT6U with 144 pins, 2Mb of flash memory and 256+4 Kbytes of SRAM.I have a little experience only with P...

Resolved! FSMC - TFT - STM32F7 Series

hi,I am trying to connect ili9341  - STM32F722ZE FSMC- TFT but i couldn't succeed .ili9342 16bit - is working in direct GPIO 16 bit data PORT drive with STM32F722ZE not in FSMC-TFT . Looks most of the ili9341 working with FMC-TFT STM32F4 Series   aro...

MMARI.1 by Senior II
  • 1149 Views
  • 1 replies
  • 0 kudos

Systick interrupt handler stopped being called

Hello STM32G0B1 For some obscure reason, sometimes the systick handler function is not called anymore.I mean, it works for some time then it does not work anymore. It looks like it is more likely to happen when I'm debugging but I have no factual inf...

JulienD_0-1723030099147.png
JulienD by Senior
  • 6934 Views
  • 13 replies
  • 3 kudos

Resolved! ST-Link V2 Connection Issue

My V2 is having communication link issues with my STVP.  It was running fine and then boom I get hit with a notification that"Cannot communicate with the device!Check the SWD cable connection and check all the needed pin connections on the SWD connec...

Resolved! Write in OSPI

Hello, I'm working on STM32H7B3I-EVAL with STM32CubeIDE. I would like to write in the OSPI, so I made the following code: void OSPI_Write(uint32_t address, uint8_t *data, uint32_t size) { OSPI_RegularCmdTypeDef sCommand; // Désactivation du mode map...

rozeelc by Associate II
  • 3656 Views
  • 7 replies
  • 0 kudos

Resolved! Does the STM32H7 FDCAN peripheral message RAM support ECC?

We're working on a new design using the STM32H753, partly based on the fact the memories have ECC implemented, but the documentation does not mention what technology is used for the FDCAN message RAM.Can someone elaborate on what protections exist fo...

mcole by Associate
  • 1778 Views
  • 2 replies
  • 0 kudos

Reg- voltage control

Hi ,      I was given a task to control the voltage value during runtime using USBPD in stm32L562CET6 board. Do you guys have any idea to start the process , I have set default value in PDO as 5 volt but the i wanted to change it simultaneously durin...

nishadh by Associate
  • 1296 Views
  • 1 replies
  • 0 kudos