STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is this MCU a fake of STM32F427VIT6?

Hi, can oneone help me to proof if the following MCU ist an original?1)The print is easier to wipe off.2)The revision number is missing or is not in the place described in the datasheet.

20240910_103406.jpg
DonFrana by Associate II
  • 2432 Views
  • 5 replies
  • 3 kudos

Resolved! no target found

I am using nucleo-144, H743ZI2 board. while i am uploading code in the stm32cubeide i am getting error as "target not found". i have searched in the community and then tried connect the boot0 to high, and power the board, connect to cube programmer a...

suhfi by Senior
  • 2640 Views
  • 1 replies
  • 1 kudos

STM32cubeIDE with stm32f103c8t6 openocd

I am new to stm32F103F103c8t6. I am using Bluepill. In OpenOCD i get:Open On-Chip Debugger 0.12.0+dev-00597-ga5a21219f (2024-06-03-11:04) [https://github.com/STMicroelectronics/OpenOCD]Licensed under GNU GPL v2For bug reports, readhttp://openocd.org/...

Resolved! UART/USART Does not Work

I would like to transmit data via USART and read the data sent to computer via a terminal(I have tried Putty and Real Term so far). To that end, I activate My USART configuration is seen as above. I also wrote the code below:uint8_t myTxData[13] = "H...

0693W00000NqsasQAB.png

Resolved! STM32G030F6P6 STMCubeProgrammer

Hi,After I program an STM32G030F6P6 I can't connect again with the STMCubeProgrammer. I have checked that my boot pin is in the correct position but still I keep on getting the error:I have used a simple program that got generated by STM32CubeIde to ...

TDie_0-1725624908750.png
T.Die by Associate II
  • 3282 Views
  • 5 replies
  • 1 kudos

Resolved! Mono chrome display with STM32 Nucleo-144

Hi,I am looking for monochorme display which can be interfaced with STM32 Nucleo-144 board. I looked into TouchGFX but it supports colored display board with this STM32 Nucleo-144 board. Can you suggest any monochomre display based board here?https:/...

mdalal by Associate III
  • 1101 Views
  • 1 replies
  • 1 kudos

STM32G473RET3 MCU

We are using STM32G473 controller for our project, In that MCU, we faced an issue in systick while using the  HAL_Delay() function.We have changed the NVIC preemption priority for Time base systick timer,Still the systick count was not incremented. W...