Question
Regarding Keil uVision5 Tool
- May 30, 2024
- 1 reply
- 1027 views
Hi friends,
I have to use Keil uVision5 Software to flash My Source code to STM32F407VET6 development board Instead of using STM32CubeIDE.But I have facing one problem during select the clock frequency of Crystal in Keil uVision5 Software that option is disable, I could not to enable the option and Unfortunately i did not set the Crystal Frequency. So ,I could not Flash source code to my Development board . I have to attach the that software error in below.