2024-05-30 3:58 AM - last edited on 2024-05-30 2:13 PM by Tesla DeLorean
Hi, I am using battery voltage charging as a part of my project. For some reasons my voltage reading in the prototype is 1.18 V and the ADC reading in my debugger is 1.25 V. This totally different for different module. Physically all modules are measuring 1.18 V across the resistors but ADC reading in debugger changes to 1.22 ,1.26,1.28.
2024-05-30 1:01 PM
What do your schematics around the STM32G0 look like?
Which ADC parameters have you set?
What does your measuring routine look like?
Without such basic information, we will not be able to help you.
Regards
/Peter