User Activity

Hi! I'm using an STM32F401RET6 and was planning on using both USART1 in Asynchronous mode and USB_OTG_FS peripherals.In STM32CubeIDE when they are configured at the same time there is an error. I've tried PA9/10 and PB6/7 for TX/RX for USART1 but the...
Hello! I've designed a PCB using STM32F407vgt6 but I cannot get it to connect using ST-LINK/V2 via the SWD interface. When I try to connect using STM32 ST-LINK Utility, I get the following error: Can not connect to target!"Connect Under Reset" mode f...
 I'm trying to port Adafruit's RA8875 Arduino library to work with an STM32F4 Discovery board. The SPI communication is failing during device initialization. During initialization, when reading the device ID register (0x0), I expect to read 0x75 but ...
I am using STM32F4 and I am trying to create 8 independent pulse outputs. I have chosen 8 timers looking at the STM32F4 Discovery datasheet and mapped them to pins. I have code for TIM2 and TIM5 that works perfectly. I change the pulse and the freque...
I have been unsuccessful in using TIM1 in Output Compare mode. I was trying to use the code that works for the general purpose timers but I cannot get it to work with the advanced timer TIM1. I read online that it is because it was an advanced timer ...
Kudos given to