Now I want to use ADC3 to collect the voltage of single-ended signals. I used IN1 channel to collect the reference voltage source of 1.5V and the internal channel to collect the internal reference voltage source of the chip respectively. The test res...
I would like to use the ADC3 of the STM32H7 series chip to realize that the voltage is collected once, and then the voltage is collected at a different point (meaning is it necessary to use two channels, because I see several channel choices in there...
STM32H7 can support SPI communication, Parallel communication, GPIO analog SPI communication, but can it support TTL, SDR CMOS, JESD204B protocol communication? Or what should I do if I want STM32 to implement these protocols?
The maximum sampling rate of STM32H743 ADC1 and ADC2 is 3.6MSPS. According to the aroma sampling principle, the maximum sine wave frequency that can be collected is 1.8MHz. I don't know if I understand it this way, right? I want to collect higher-fre...
The number of bits shown in the data manual is 12.2 bits, with an error of 20LSB. I used a reference voltage source of 3V, and the error between the ADC value obtained and the actual value is about 10mv. Is this scientific? How big should the theoret...