STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Rebroadcasting existing CAN msg on network issue

I'm working with an existing CAN network on which I want to read a msg, modify it slightly and rebroadcast.I'm running into an issue where the code seems to crash/freeze if I broadcast the new message too close to the original one thats on the networ...

pulsar by Associate II
  • 1990 Views
  • 4 replies
  • 0 kudos

Recovering STM32H563 from closed product_state

Hey community, I was working on some production scripts for our H5 based boards and got myself locked out.This occured after trying to set the obk file. STM32_Programmer_CLI -c port=SWD ap=1 -sdp=<wrong_obk_path> I got a corresponding warning "Error:...

Schue by Associate II
  • 1645 Views
  • 2 replies
  • 0 kudos

GPIO mode change

Hi,  I set it to GPIO Input mode and am using it. When I receive any signal during MCU operation, I want to convert it to Input -> EXTI mode. I wrote these codes at the moment, but there seems to be a problem. My Init code :  GPIO_InitStruct.Pin = ...

giwonKIM by Associate III
  • 1557 Views
  • 2 replies
  • 2 kudos

stm32f072rbt6 discovery board spi issue

Hello everyone,I am working with the STM32F072RBT6 Discovery board, where the board is configured as an SPI slave while another device acts as the master. I am utilizing DMA to receive and transmit data through two SPI interfaces (SPI1 and SPI2).Curr...

Resolved! USB - RNDIS

HI team,               I am using STM32F769 board , do we have sample code or example for USB RNDIS application for F7 series. 

Shikamaru by Associate III
  • 1698 Views
  • 2 replies
  • 1 kudos

STM32U Series Ultra Low Power No-Vref Pin

Hi friends. With using STM32U535 microcontroller, i plan to make a project. The project includes 3.6V battery cell. We read adc values when this battery cell supplies the microcontroller. When the battery voltage decreases, the reference voltage shou...

How to configure Ethernet with four MACs in STM32H745?

HI, AS mentioned in Reference Manual (RM0399) we can configure Four mac addresses. We are trying to configure four MAC's in stm32h745 ,we have configured two mac address successfully ,and we are unable to configure the remaining two mac addresses.so ...

syed1 by Associate II
  • 1546 Views
  • 2 replies
  • 1 kudos

Resolved! STM32G4 TCXO

Please let me know if there are any hardware or sofware specifics for connecting TCXO to the STM32G474 series? What should pay special attention to?I use FT2MN at 40 MHz. Its output was connected through a 10 pF capacitor and a 220 Ohm resistor, in s...

CrazyChel by Associate III
  • 10270 Views
  • 25 replies
  • 8 kudos