STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error at start of debugging while Flash write test

I am testing Flash write using a custom board with STM32H562VG.For debugging, I use IAR I-jet and VSCode's C-SPY extension.The following HAL API is used for Flash writing, addr starts at 0x08030000 in the User area.HAL_FLASH_Program(FLASH_TYPEPROGRAM...

Thoufiel by Associate III
  • 1586 Views
  • 2 replies
  • 0 kudos

Resolved! DMA and GPIO on STM32C031G6

I would like to sample the entire GPIOA Port using the DMA and TIM16. TIM16 triggers the DMA which in turn is supposed to copy the content of the IDR register of GPIO onto an array. This works fine if I use the CNT register of TIM16 as CPAR. When I s...

areum by Associate
  • 1134 Views
  • 1 replies
  • 1 kudos

unable to write in flash memory.

Hi, i am using STM32G0C1RET6 MCU board, i am unable to write in flash memory. i am using an 8 byte structure to put data at that location. but I don't know what is going wrong. please, help... I have given some part of the code below,   static FLASH_...

Rohit007 by Associate III
  • 2235 Views
  • 5 replies
  • 1 kudos

RC filter before ADC

Previously through testing using fast channal, single-ended input can realize less than 1.5M sinusoidal FFT, I want to add RC filter on the input, but I don't know what is the limitation for RC selection? Please help me, the cutoff frequency of the r...

hanqingze_0-1727154534413.png
hanqingze by Associate III
  • 3072 Views
  • 4 replies
  • 1 kudos

[STM32L4] Hard fault during OSC32_OUT init as GPO

I want to use the OSC32_OUT Pin (PC15) of the STM32L432KC as general purpose output. Moreover i connected a FET with a pullup to this pin and want to control them. I do not use any LSE oscillator functionality. The datasheet states that upon reset th...

Syn_BE by Associate III
  • 3515 Views
  • 5 replies
  • 0 kudos

STM32H7R3I8K6 vs STM32H750IBK6 current draw?

I'm trying to get a ballpark estimate of what sort of current draw consumption I can expect if we migrate to the H7R3, which uses a SMPS for the core, as opposed to the built-in LDO for the core on the H750.Is there a place I can compare the current ...

External QSPI flash programming using JLink

Dear All,Currently I am trying to load some code to the STM32U599NJH6Q that is interfaced with the MT25QL128ABA QSPI flash over the OCTOSPI2 peripheral, using a JLink programmer.The pinout of this peripheral on my custom PCB is:I have also checked th...

G_Anastasopoulos_0-1721736293186.png G_Anastasopoulos_1-1721736456038.png G_Anastasopoulos_2-1721736631933.png

Data logging and controlling STM devices via computer

Hello Everyone,I'm about to start a new project where I have some products built on STM32.Now I wanted to connect those devices to the microsoft widows based computer and build a windows software to control the devices and get the stored data from de...

prathmesh by Associate II
  • 4244 Views
  • 9 replies
  • 1 kudos