STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I cant download anyrhing from ST website

When i try to download STM32CubeMx from ST website nothing happens.https://www.st.com/en/development-tools/stm32cubemx.htmlI press "Get latest", than i log in my ST account, press "Get latest" again and nothing happens. I have no proxy on my  compute...

IvanEZZ by Associate
  • 1236 Views
  • 1 replies
  • 2 kudos

Resolved! Nucleo F746ZG PC13 User Button Triggering Interrupt on Init

I have a Nucleo 144-pin F746ZG and I want to configure the user button (PC13, pulled to ground according to MB1137 schematic) to toggle an onboard LED on a falling edge via EXTI interrupt.I am using this sequence to initialize the interrupt handling:...

PC13_UserButton.png
JS5 by Associate II
  • 2556 Views
  • 3 replies
  • 1 kudos

Resolved! I2C Issue between two H7 Dev Boards

Hi, I've been trying to get an i2c connection working between two nucleo boards however nothing i have tried has worked. i am using the NUCLEO-H755ZI-Q and the NUCLEO-H723ZG both with i2c1 and on the same pins pb8(scl) and pb9(sba). for the H755 dual...

voxe_0-1727421627953.png voxe_1-1727421824098.png voxe_2-1727421838542.png
voxe by Associate II
  • 2444 Views
  • 4 replies
  • 4 kudos

Firmaware demo for STM32H73LI-DK

Hello, Hello,I purchased an STM32h7b3LI-DK demo board and I would like to have the source codeof the demo firmware installed on the board, is this possible?Best regardsSébastien     

PSEBA.1 by Associate II
  • 921 Views
  • 1 replies
  • 0 kudos

Resolved! FDCAN not working with STM32U5F7

I'm using a custom board with an STM32U5F7. Written a program(with nothing else configured other than clock and FDCAN) that simply sends out a message via FDCAN (in classis mode, 500kbps) which I'm hoping to receive using a P-CAN. When probing the TX...

Hareesh_S by Associate III
  • 8225 Views
  • 21 replies
  • 0 kudos

Resolved! How to generate a timestamp for datalogging ?

I need to generate a timestamp for data logging, but I'm not sure how to do it.The data packets are received via the UART at a 100ms rate and each packet of data consists of 10 bytes of serial dataByte 0: TemperatureByte 1: Voltage high byteByte 2: V...

johngj by Senior
  • 5771 Views
  • 5 replies
  • 2 kudos

Resolved! Can't get oneshot timers to work

I want tim16 to, every 1 second, start tim15 which is a oneshot timer which then does something when the period elapsed.I start tim16 in my main function, which works correctly, but the tim15 interrupt only triggers once, so my output looks like this...

DavidL_ by Associate III
  • 1053 Views
  • 1 replies
  • 0 kudos