Skip to main content
Visitor II
June 25, 2024
Question

The values ​​read back by STM32 HAL_SPI are all 0x00

  • June 25, 2024
  • 0 replies
  • 806 views

At present, when STM32L412 uses the HAL_SPI command to read back the Register, no matter which Register is used, it is 0, but it is normal to use LA to read the data. The waveform is as follows:

RayWang_0-1719306626148.png

Is there any unprocessed program that causes the SPI reading values ​​to be all 0? please help. Thanks!

Below is the current program for reference.

ads131m0xTxBuff[0] = (ads131m0x_CMD_RREG | (0x00<<7)) >> 8;
ads131m0xTxBuff[1] = (ads131m0x_CMD_RREG | (0x00<<7)) & 0xFF;
ads131m0xTxBuff[2] = 0x00;
ads131m0xTxBuff[3] = 0x00;
ads131m0xTxBuff[4] = 0x00;
ads131m0xTxBuff[5] = 0x00;

while(HAL_SPI_GetState(&hspi2) == HAL_SPI_STATE_BUSY);
HAL_GPIO_WritePin(SPI2_NSS_GPIO_Port, SPI2_NSS_Pin, GPIO_PIN_RESET);
while(HAL_SPI_GetState(&hspi2) != HAL_SPI_STATE_READY);
HAL_SPI_TransmitReceive(&hspi2, ads131m0xTxBuff, ads131m0xRxBuff, 3, 10);
while(HAL_SPI_GetState(&hspi2) != HAL_SPI_STATE_READY);
HAL_GPIO_WritePin(SPI2_NSS_GPIO_Port, SPI2_NSS_Pin, GPIO_PIN_SET);

 

while(HAL_SPI_GetState(&hspi2) == HAL_SPI_STATE_BUSY);
HAL_GPIO_WritePin(SPI2_NSS_GPIO_Port, SPI2_NSS_Pin, GPIO_PIN_RESET);
while(HAL_SPI_GetState(&hspi2) != HAL_SPI_STATE_READY);
HAL_SPI_Receive(&hspi2, ads131m0xRxBuff, 3, 100);
adc_status = ads131m0xRxBuff[0] <<8;
adc_status |= ads131m0xRxBuff[1] &0xFF;
while(HAL_SPI_GetState(&hspi2) != HAL_SPI_STATE_READY);
HAL_GPIO_WritePin(SPI2_NSS_GPIO_Port, SPI2_NSS_Pin, GPIO_PIN_SET);

 

Any advice and advice would be greatly appreciated. Thanks!

This topic has been closed for replies.