STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G0 TX Busy Flag Set when ClockPrescaler is 8

Hi, HAL_UART_STATE_BUSY_TX is always Set when I change the ClockPrescaler of USART Paremeter.My Cube configurations are in photo above. I have to drive Usart with 100 Baudrate. Systemclock Frequency is 50Mhz.  When SystemClock is 50Mhz and ClockPresc...

gceti1_0-1728306451623.png gceti1_1-1728306542177.png
gceti.1 by Associate II
  • 2069 Views
  • 4 replies
  • 0 kudos

STM32G474 HRTimer, Dead time And Duty Cycle

Hi all! Hoping someone can help me with this. Right now, I have Timer A and Timer B as my main outputs; Timer A controls one set of switches in my half bridge, and Timer B controls the other half. I have one "mode" set, where I can adjust the phase s...

Jbin0101 by Associate III
  • 3197 Views
  • 2 replies
  • 0 kudos

Resolved! STOP mode F405 hard to come down 1mA

Hi all,I'm trying to acheive STOP mode on my stm32f405, but ir's hard to come down 1mA as de datasheet say < 100uA. So to explain my project :- STM32F405 Freertos- 3 i2c capteur (power of captor is managed by switch)- 1 spi flash nand w25n01My clock ...

SBaro.11 by Associate III
  • 2055 Views
  • 4 replies
  • 1 kudos

Resolved! STM32H7 traceclkin source

Hi all,I'm trying to understand what source the STM32H7 (specifically STM32H743) uses for the TPIU trace clock.According to the RCC chapter there ought to be a multiplexer that allows to choose from a number of sources:According to the debug chapter,...

drath_0-1728309614149.png drath_1-1728309679906.png
drath by Associate
  • 2143 Views
  • 3 replies
  • 0 kudos

HT7533 can be used for STM32F105RBT6 power supply?

Many engineers I know use HT7533 as power supply for STM32F105RBT6 in automotive boards. I looked up the specs, and found that HT7533 is only rated for 100mA. Is it too low for STM32F105RBT6? Is TI's TPS7B91 or TPS7B92 better in this case? Thank you.

ax369 by Associate II
  • 1088 Views
  • 1 replies
  • 0 kudos

STM32H723VGT6 chip cannot erase and upload programs

  Hello everyone, Using the STM32H723VGT6 chip, the program can be downloaded and run normally, but cannot be erased and uploaded, prompting "Error while determining flash info (Bank 1 @ 0x90000000) Failed to read back". The same phenomenon occurs wh...

STM32H723VGT6.png
XYN by Associate
  • 1187 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H725 Bulk capacitors values

Hello all,Regarding the STM32H725 bulk capacitors:Question 1:Is the capacitors required values taken into consideration the capacitance degradation Vs DC bias?For example:The SMPS input required is 4.7uF (10uF recommended)Looking at the STM32H735G-DK...

NirAlon_0-1728837166758.png
NirAlon by Associate III
  • 2591 Views
  • 4 replies
  • 0 kudos