2024-07-05 12:21 AM
void tcpsend (char *data)
{
// send the data to the connected connection
netconn_write(conn, data, strlen(data), NETCONN_COPY);
// relaese the semaphore
sys_sem_signal(&tcpsem);
}
//
//void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
//{
// // a++;
// if(UartHandle->Instance == UART5)
// {
// //if (a%100==0)
// // HAL_UART_Transmit(&huart3, (uint8_t *)rxd, 1, 0xFFFF);
// // HAL_UART_Receive_IT(&huart5, rx_buffer, ROVER_MSG_LEN);
// HAL_UARTEx_ReceiveToIdle_IT(&huart5, rx_buffer, ROVER_MSG_LEN);
// }
//}
static void tcpsend_thread (void *arg)
{
MX_UART5_Init();
while (1)
{
//rx_buffer[1]=1;
//tcpsend(rx_buffer[1]);
osDelay(200); //2000 or 5000
// Enter task section
//__disable_irq();
// UART reception
HAL_UARTEx_ReceiveToIdle_IT(&huart5, rx_buffer, ROVER_MSG_LEN);
// __HAL_UART_DISABLE_IT(&huart5,UART_IT_RXNE);
//ulTaskNotifyTake(pdTRUE , portMAX_DELAY);
if (g_rxSize <= 0)
continue;
//__HAL_UART_ENABLE_IT(&huart5,UART_IT_RXNE); // Exit critical task section
int i;
int j;
volatile int len_gpgga=0;
volatile int len_gpgst=0;
for(int x=1;x<ROVER_MSG_LEN; x++){
if(rx_buffer[x]==0x24){
len_gpgga=x;
for(int y=len_gpgga; y<ROVER_MSG_LEN;y++){
if(rx_buffer[y]==0xB5){
len_gpgst=y- len_gpgga;
break;
}
}
break;
}
}
for(i=0; i<ROVER_MSG_LEN; i++){
if (rx_buffer[i] == 0x24 && rx_buffer[i+1] == 0x47){
if (rx_buffer[i+3] == 0x47 && rx_buffer[i+4]== 0x47 ){
if(rx_buffer[i+5]== 0x41){
memcpy(&gpgga, &rx_buffer[i], len_gpgga);
gpgga[2]= 'P';
}
}
}
if (rx_buffer[i] == 0x24 && rx_buffer[i+1] == 0x47){
if (rx_buffer[i+3] == 0x47 && rx_buffer[i+4]== 0x53 ){
if(rx_buffer[i+5]== 0x54){
// Packet is valid, copy the data
memcpy(&gpgst, &rx_buffer[i], len_gpgst);
gpgst[2]= 'P';
}
}
}
if(rx_buffer[i] == 0xB5){
if(rx_buffer[i+1] == 0x62){
if(rx_buffer[i+2] == 0x01){
if(rx_buffer[i+3] == 0x3c){
if (rx_buffer[i+4] == 64){
uint8_t calculatedCK_A = 0;
uint8_t calculatedCK_B = 0;
for (j = i+2; j < i+72 - 2; j++)
{
calculatedCK_A += rx_buffer[j];
calculatedCK_B += calculatedCK_A;
}
if (calculatedCK_A == rx_buffer[i+72 - 2] && calculatedCK_B == rx_buffer[i+72 -1])
{
memcpy(&zedf9pData, &rx_buffer[i+6], sizeof(ZEDF9P_Data));
uint8_t message[100];
sprintf(message,"$GPHDT,%lu,T",zedf9pData.relPosHeading);
int crc = nmea_checksum(message);
sprintf(message+strlen(message),"*%X\r\n",crc);
sys_arch_sem_wait(&tcpsem, 500);
memset(rx_buffer, 0, sizeof(rx_buffer));
for (int e = 0; e<len_gpgst;e++){
merged[e] = gpgst[e];
}
for (int e = 0; e<300;e++){
merged[e+len_gpgst] = message[e];
}
if (gpgga[3]=='G'){
tcpsend(gpgga);
osDelay(200);
if (merged[3]=='G'){
tcpsend(merged);
osDelay(200);
}
}
memset(gpgga, 0, sizeof(gpgga));
memset(gpgst, 0, sizeof(gpgst));
memset(message, 0, sizeof(message));
break;
}
}
}
}
}
}
}
// HAL_UART_RxCpltCallback(&huart5);
}
}I am trying to get continuous data flow from ethernet but when I change processor clock It does not work. Should it be dependent to processor clock or how can i make independent? I guess I am having trouble about the code flow. How should I be using receive function if that is the problem?