User Activity

I'm using an STM32H743VIT6 (rev V in LQFP100 package), powered at 3.3V and programmed with STM32CubeIDE.I'm using the ADC2 and ADC3, and also want to use the VREFBUF voltage (available on VREF+ pin) programmed for 2.5V. The *.ioc file is generated wi...
I use the STM32CubeIDE program on Mac (Version 1.15.0)The MCU is a STM32H743VIT and its configuration is done from the *.ioc file.I use ADC3 with an Oversampling of 128.Its configuration is done by entering 128 for the “Oversampling Ratio” line, and ...
Kudos from