STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with erasing and overwriting FLASH data

Posted on June 15, 2013 at 12:58Hi,After writing in FLASH using FLASH_ProgramWord(uint32_t Address,Data). I can't overwrite that address data completely using FLASH_ProgramWord(Address,0xFFFFFFFF) or FLASH_ProgramWord(Address,Newdata);.In case of er...

Using ST FSMC_SRAM_DataMemory example on keil

Posted on June 14, 2013 at 12:41I cannot find the startup file and scatter file for Keil for FSMC_SRAM_DataMemory example in STM32F4xx_DSP_StdPeriph_Lib_V1.1.0.Basically i want to use external memory on STM3240G eval  board as my stack and heap spac...

rishi2 by Associate III
  • 2300 Views
  • 4 replies
  • 0 kudos

ADC GPIO pin pairing for STM32F407

Posted on June 14, 2013 at 23:22Can someone tell me the paring for all ADC channels and GPIO ports for the STM32F407? I've seen some of the pairings in posts here (such as PA0 for channel 0, CA2 for channel 12), but I need a complete list. I'm sorry...

cwparker by Associate II
  • 1298 Views
  • 1 replies
  • 0 kudos

CMSIS DSP matrix inverse

Posted on June 08, 2013 at 01:32 Hi, i realized a test source code for matrix inversion. I used the CMSIS DSP library which include arm_mat_inverse_f I also took a look at arm_matrix_example_fc... but i had 1 problem and 1 question. ...

dario by Associate II
  • 2572 Views
  • 2 replies
  • 0 kudos

Nonvolotile EEPROM for configuration parameters

Posted on June 14, 2013 at 07:20In old good 8-bit Architecture (AVR,PIC,...) CPU had a nonvolatile memory region to keep configuration parameters of the application that were persistent over reset. This region had a byte read/write access without er...

dimax by Senior
  • 2017 Views
  • 5 replies
  • 0 kudos

Is STM32F427 pin to pin compatible with STM32F407

Posted on June 14, 2013 at 08:46Hi, The F4 series discovery card uses STM32F407. For our project we are considering using STM32F427. I'm wondering if they are pin to pin compatible? Thanks Michale #stm32 #discovery

myshen by Associate
  • 988 Views
  • 1 replies
  • 0 kudos

stm32 adc multi channel

Posted on June 08, 2013 at 12:15The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32F103 internal temperature sensor

Posted on June 11, 2013 at 14:12Hi! I have seen an earlier discussion with the device stm32F051 or F205 regarding the TS_CAL1 and 2 values. My question is, are these values applicable for the STM32F103 device? Cannot find any references to them in t...

peter23 by Associate II
  • 3780 Views
  • 8 replies
  • 0 kudos