User Activity

Hi, I purchased the SensorTile.box PRO sensor, but I can't develop because it doesn't connect to the STLINK V2-1, in the datasheet it says:I connect adapter STEVALMK1 (that was inside the kit) with STLINK V2-1But I have the following error  the docum...
I'm working with the STEVAL-SPIN3201 boardI have compiled and uploaded example "6s_STEVAL3201_HS_VM"I have a 70mm diameter sensored BLDC motorWhen I connect through the software ST Motor Pilot V0.9.9 click in "Start" Motor and the motor turns 1/4 tur...
I am working with BlueNRG LP.I am acquiring 3 channels:ADC_VINP0 (PB3)ADC_VINM0 (PB2)BATTERY.I used and modified example of the "BlueNRG-LP Navigator" ADC_DMA.I read ADC_VINP0 and the batteries but ADC_VINM0 not work!! ( I used STEVAL-IDB011V1 and i ...
I'm using this device. with "BlueNRG-1_2 DK 3.1.0"I have a problem with reading ADC.use two channels pin1, pin2 (ADC1, ADC2), connected to two potentiometers (analog joystick)I can read only one channel, how can I read the two channels?In this code t...
Kudos from