STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32 programing problem

Posted on June 16, 2013 at 12:38I'm using IAR. My board wold not get programated. In fact the program annonce that the program was successfully downloaded and the debug mode is opned but the program in the stm32 wold not change :\ when I chek the de...

Internal Sram Read And Write

Posted on June 16, 2013 at 06:32Hey guys,I would be very grateful if someone help me for the following issue.I want to compile and save some information in an indoor internal SRAMmicrocontroller when power supply of microcontroller goes offline,thos...

htc by Associate
  • 1001 Views
  • 1 replies
  • 0 kudos

STM32F2xx Bootloader Sectors allocation

Posted on June 15, 2013 at 08:00HI, I'm starting to implement my own bootloader for STM32F2xx. Currently I plan to support UART, USB and ETH. Also I plan to use EEPROM emulation. Implementation of USB and ETH (TCPIP Socket) takes about 30K. So To b...

dimax by Senior
  • 2549 Views
  • 9 replies
  • 0 kudos

Where is the NVIC_InitStructure?

Posted on June 15, 2013 at 22:18I am trying to configure the NVIC for the first time. In looking online for help, most project reference these functions:   NVIC_InitTypeDef NVIC_InitStructure;   /* Enable the TIM2 gloabal Interrupt */   NVIC_InitStr...

STM32 HS USB DMA Transfer

Posted on May 14, 2013 at 23:02Is it possible to use DMA for USB transfers? My understanding of the STM32 DMA controller is that it will transfer data from one place to another without CPU usage. If I were moving data from RAM to a DAC output, I can...

ckern by Associate II
  • 3009 Views
  • 3 replies
  • 0 kudos

STM32F4xx Bootloader and Security

Posted on June 15, 2013 at 13:18I wrote my bootloader, that load application to the flash. Now I want to set security. Is it enough to set RDP Level1 and write protection to sector0, where my bootloader is located? Or I need to set RDP to Level2? Th...

alexandr by Associate II
  • 1227 Views
  • 2 replies
  • 0 kudos

How to define the GPIO mode ?

Posted on August 13, 2012 at 09:20typedef enum { GPIO_Mode_AIN = 0x0,   GPIO_Mode_IN_FLOATING = 0x04,   GPIO_Mode_IPD = 0x28,   GPIO_Mode_IPU = 0x48,   GPIO_Mode_Out_OD = 0x14,   GPIO_Mode_Out_PP = 0x10,   GPIO_Mode_AF_OD = 0x1C,   GPIO_Mode_AF_PP =...

614678489 by Associate II
  • 9583 Views
  • 10 replies
  • 0 kudos

WiFi query

Posted on March 12, 2013 at 06:40Hi, Anyone of you have worked on WIFI? I need a small help related to that. I am using Hi-Link WIFI module named HLK M03 WIFI module with STM32 controller. I am able to configure my WIFI module properly i.e. initiali...

manoj23 by Associate II
  • 3471 Views
  • 10 replies
  • 0 kudos