STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Building CT-VPD dongle with ST products

Hi all.Are there any guides on building the charge-through VPD device with the ST product? An illustration from the standard: The goal is to maintain the smartphone's supply from the external PD charger while maintaining the connection with a USB 2.0...

VasylV_2-1727761563566.png
VasylV by Associate
  • 2095 Views
  • 3 replies
  • 1 kudos

Resolved! STM32F105xx SPI2 Does Not Drive NSS Pin High when Idle

I'm using the ST Cube environment (IDE + MX) to configure the SPI2 peripheral in Full-Duplex Master mode on a STM32F105VBHX chip.It seems like the peripheral is not driving the NSS (chip select) pin (PB12).  When the pin is selected for SPI2_NSS and ...

Brian H by Senior
  • 4684 Views
  • 8 replies
  • 5 kudos

target is not responding, retrying

I have a program with various tasks, in one of these I send a request and, after that, I wait for a response, so I have a cycle like this SendRequest(); do { WaitResponse(); DelayMillisecondS(200); }while (Timerisnotexpired()); the Problem is that th...

IVent.1 by Senior
  • 1535 Views
  • 2 replies
  • 0 kudos

Resolved! UST OTG configuration

Hi,I am thinking using the STM32U5G9VJT6Q and configure the USB to USB-OTG but never used USB OTG before.The PCB would have its own power supply and only work when power is applied through it and never take power from the USB connector. The USB would...

Ricko by Senior III
  • 1442 Views
  • 1 replies
  • 0 kudos

Resolved! CAN bus not looping NUCLEO-F767zi

Hello! I followed this video for CAN-bus https://www.youtube.com/watch?v=JfWlIY0zAIc&t=918s but as simply as it looks, my configuration doesnt seem to work, I'm working on the NUCLEO-F767zi, I started a new project with default config simply adding C...

vFazzi by Associate
  • 2446 Views
  • 3 replies
  • 2 kudos

B-G473E-ZEST1S + power board

I recently saw your presentation of HSO in motor control.I have a couple of questions:1) Is the HSO algorithm implementable in the B-G431ESC board? (It seems to me no..)2) I have a 48V motor and about 20-30A rms which is obviously not controllable by...

luke514_0-1730727181817.png
luke514 by Senior
  • 903 Views
  • 0 replies
  • 0 kudos

IAP Jump to application not working

Hello, IAP have problem that jump to app.MCU : Stm32f303cbt6 - boot sidea. STM32F303CBTX_FLASH.ldb. main.cc. main.h  - app sidea. STM32F303CBTX_FLASH.ldb. system_stm32f3xx.c Thanks. 

TaronKim_0-1730683594916.png TaronKim_1-1730683631898.png TaronKim_3-1730683694730.png TaronKim_2-1730683661036.png
TaronKim by Associate II
  • 3237 Views
  • 6 replies
  • 0 kudos

STM32L552ZET6Q Sleep Mode Issue?

Hello,    We are using STM32L552ZET6Q MCU in our project. Here we are using only 3 UART Pheripherals, 2 LED output GPIOs.    Here We attached the CUBEMX .ioc file of the our project. After the code generation from the STM32CUBEMX, we complete our's o...

STM32L552ZET6Q.jpeg

Resolved! STM32F103x8 pin compatible or LQFP48 alternative

Hi all,I've a board with the STM32F103C8T6 MCU.My firmware has to handle a lot of IO, display and UART logic, nothing special but just a lot of logic.So the 64K b internal flash memory is almost full.I've a couple of question here:1) can i switch to ...