STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem using NVIC_SetVectorTable on StmF3Discovery

Posted on November 22, 2013 at 00:44Hi there, I've got a problem here using NVIC_SetVectorTable(). I have attached my test programm, which is held very simple and does: - Init Leds&UserButton - make sure the ''new'' Vectortable is 0x200-aligned - Co...

STM32F303CB ==> RCC_ADCCLKConfig

Posted on November 21, 2013 at 16:23Hello, I have a problem with the RCC_ADCCLKConfig, I want to change the  ADC frequency and I followed the example from st.    /* Configure the ADC clock */   RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div64);     /* Enable...

stm32 I2s in slave mode Timing

Posted on November 22, 2013 at 11:57 The stm32 chip has a error for I2S in slave mode (stm32f40x Errata sheet 2.4.1). 2.4.1 In I2S slave mode, WS level must be set by the external master when enabling the I2S Description In slave mode, th...

Is there a way to reset SPI RxFifo?

Posted on November 21, 2013 at 15:25Hi, I would like to ask if there is a way to clear the FRLVL and RXNE bits in SPIx->SR in order to ignore everything that has been received before. I have some routines that only send data and other that will als...

mmensch by Associate II
  • 901 Views
  • 3 replies
  • 0 kudos

hard fault handler

Posted on August 04, 2013 at 01:47hi,i am working on stm32f407. i am experiencing hard fault handler. start:{}timer();while(!one_second_timer){ /*my code*/}goto start;and the code for timer is void timer(void){ uint16_t PrescalerValue = 0; TIM_Cmd(T...

bilal by Associate II
  • 1761 Views
  • 3 replies
  • 0 kudos

STM32F205 __disable_irq() undefined symbol Keil ARM

Posted on November 20, 2013 at 08:43Hi. I want to disable all interrupts in my STM32F205  and I use macro __disable_irq() in core_cmFunc.h. I verified that this instructions works fine, but in ARM Keil IDE, if I select ''Go to definition of __disab...

giovanni by Associate
  • 2881 Views
  • 3 replies
  • 0 kudos

Bug in USB library v4.0.0 usb_prop.c

Posted on November 21, 2013 at 01:28 I've come across an issue in usb_prop.c in the STM32 USB library examples. The _GetStringDescriptor function checks for the index of the Descriptor string, but allows an index of up to 4. There are actually o...