cancel
Showing results for 
Search instead for 
Did you mean: 

Basic USART Communication

aru
Associate II
Posted on February 05, 2013 at 08:41

I am using stm32f107rct6 with 25Mhz freq for usart communication. i am sending character 'a' from PC but i am receiving some unwanted data like 'FE' and i am receiving the same data no change , so pls let me known why is this happening , i have tested the same code in  stm32f103rb series in 8Mhz frequency its working fine 

 the configuration and the code  i have done is shown below ,plz solve this as early as possible and its very critical , it is an online project.even i have attached the .c-file

#include<stdio.h>

#include<stm32f10x_lib.h>

void RCC_Config(void);

void GPIO_Config(void);

unsigned int temp,x;

char ch;

main()

{  

RCC_Config();

// SystemInit();

GPIO_Config();

USART1->BRR=0x341;//0xA2C; //9600 baud rate

USART1->CR1=0x0000006D; //TCIE &RXNEIE(read data reg not empty interrupt enable)

USART1->CR2=0x000;   //eable clock

USART1->CR1|=0x2000;

NVIC->ISER[1] = 0x25;//USART1_IRQChannel //(1 << (USART1_IRQChannel & 0x1F));//0x00000020;

USART1->CR1|=0x00002000;

while(1)

{

;

}

 }

void RCC_Config(void)

{

RCC->APB2ENR=0x00004004;

}

void GPIO_Config(void)

{

 AFIO->MAPR=0x00000000;

 GPIOA->CRH = (GPIOA->CRH & 0xFFFFF00F)|0x4B0;

}

  

void USART1_IRQHandler(void)

{

if ((USART1->SR & 0x20))

{

temp=1;

ch=USART1->DR;

x=USART1->SR;

}

else if ((USART1->SR & 0x40))

{

if (temp==1)

{

x=USART1->SR;

temp=0;

USART1->DR=ch;  

}

}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on February 05, 2013 at 14:03

Check the clock and PLL settings, and confirm the CPU is running at the frequency you expect, use the MCO pin if required.

Invalid data rates almost always relate to a mismatch between actual and assumed clocks.

If you were using the library the HSE_VALUE would be critical. The CMSIS library calls SystemInit() prior to main()
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..