Skip to main content
pietro2
Associate III
February 4, 2013
Question

I2c on STM32f0Discovery

  • February 4, 2013
  • 1 reply
  • 401 views
Posted on February 04, 2013 at 11:18

Good morning, i need to develop an application that read and write informations (like a mac address)between an stm32f0discovery board and a 24c02 EEprom, i need to use the PB8 and PB9 pins ad SCA and SCL.

If someone have suggestion like example codes or hardware setup are welcome.

Thanks.

#i2c-stm32f0discovery
This topic has been closed for replies.

1 reply

pietro2
pietro2Author
Associate III
February 5, 2013
Posted on February 05, 2013 at 16:54

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6W1&d=%2Fa%2F0X0000000bpg%2F2WXZLVaHayXL6bV9xPMm0tGi3mmbtxYvDqdjJtIACj4&asPdf=false