cancel
Showing results for 
Search instead for 
Did you mean: 

HIGH SPEED GPIO PROBLEM

xtian
Associate II
Posted on February 01, 2013 at 16:04

Hi Guys,

I have a question, I have this code and the TTL logic interface that I am reading has a speed of about 1Us The problem is.. I am not able to read all of the 1Us Data.. do you have suggestions how to tweak my code? for now I am using serial to view my data..as I am just in the process of studying SPI and SDIO


#include ''stm32f10x.h''

#include ''stdio.h''

#include ''stm32f10x_conf.h''

#include ''stm32f10x_spi.h''


#define BufferSize 32

typedef enum {FAILED = 0, PASSED = !FAILED} TestStatus;


/* function prototypes */ 

void RCC_Configuration(void);

void GPIO_Configuration(void); 

void USART_Initialization(void);

void SPI_Initialization(void);

void resetDataAndCounter(void);

void SendData(void);


/* structure with data for USART configuration */ 

USART_InitTypeDef USART_InitStructure; /* HW configuration */ 

SPI_InitTypeDef SPI_InitStructure;

GPIO_InitTypeDef GPIO_InitStructure; 


SPI_InitTypeDef SPI_InitStructure;

uint8_t SPI_MASTER_Buffer_Tx[BufferSize] = {0x01, 0x02, 0x03, 0x04, 0x05, 0x06,

0x07, 0x08, 0x09, 0x0A, 0x0B, 0x0C,

0x0D, 0x0E, 0x0F, 0x10, 0x11, 0x12,

0x13, 0x14, 0x15, 0x16, 0x17, 0x18,

0x19, 0x1A, 0x1B, 0x1C, 0x1D, 0x1E,

0x1F, 0x20};

uint8_t SPI_SLAVE_Buffer_Rx[BufferSize];

__IO uint8_t TxIdx = 0, RxIdx = 0;

volatile TestStatus TransferStatus = FAILED;

ErrorStatus HSEStartUpStatus;


int datas[30];

int ctr = 0;


int main(void) 

{ 

RCC_Configuration(); 

GPIO_Configuration(); 

USART_Initialization();

SPI_Initialization();

resetDataAndCounter();


while (1)

{


int PortsData = 15- GPIOA ->IDR >>8 & 0x000F;


if (PortsData == 10)

{

int DIOData = 255 - GPIOC ->IDR>>0 & 0x00FF;

if ((DIOData > 64)&&(DIOData <=96))

{

datas[ctr] = DIOData;

USART_SendData(USART2, datas[ctr]);

};

ctr++;

while (PortsData !=6)

{

PortsData = 15 - GPIOA ->IDR >>8 & 0x000F;

}

}


if ((ctr==30))

{

//send DATA;

SendData();

ctr = 0;

resetDataAndCounter();

}

}

}


void resetDataAndCounter(void)

{

ctr = 0;

for (int ctr1 = 0; ctr1 <30; ctr1++)

{

datas[ctr1] = 0;

}

}


void SendData(void)

{

for (int ctr1 = 0; ctr1<30; ctr1++)

{

USART_SendData(USART2, datas[ctr1]);

for (int ctr2=0; ctr2<=1024; ctr2++);

}

USART_SendData(USART2,44);

}


void RCC_Configuration(void) 

{ 

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); 

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE); 

} 


void GPIO_Configuration(void) 

{ 

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; 

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz; 

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; 

GPIO_Init(GPIOA, &GPIO_InitStructure); 


GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12; 

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPD; 

GPIO_Init(GPIOA, &GPIO_InitStructure);


GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; 

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; 

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; 

GPIO_Init(GPIOC, &GPIO_InitStructure); 


GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7 ; 

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPD; 

GPIO_Init(GPIOC, &GPIO_InitStructure); 


}

void USART_Initialization(void)

{

USART_InitStructure.USART_BaudRate = 115200; 

USART_InitStructure.USART_WordLength = USART_WordLength_8b; 

USART_InitStructure.USART_StopBits = USART_StopBits_1; 

USART_InitStructure.USART_Parity = USART_Parity_No ; 

USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; 

USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; 

USART_Init(USART2, &USART_InitStructure); 

USART_Cmd(USART2, ENABLE); 

}


void SPI_Initialization(void)

{

SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;

SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;

SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64;

SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

SPI_InitStructure.SPI_CRCPolynomial = 7;

SPI_Init(SPI1 , &SPI_InitStructure);

SPI_Cmd(SPI1, ENABLE);

}

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on February 01, 2013 at 16:12

The USART output routines seem to ignore the need to wait on the register to be empty.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
xtian
Associate II
Posted on February 01, 2013 at 16:24

HI Clive thanks for your update... so there's nothing wrong with my GPIO code? its fully optimized?

ahh this one-USART_SendData(USART2, datas[ctr]); I just Forgot to remove it I was trying to troubleshoot why I can't read the microseconds data and it turns out that I was not able to read it for example the controller sends a ABCDEFG, with the ''the one I forgot to remove'' it is showing sometime A sometime D in other words random I always wait 5 seconds before I send Data.. still same.. all RANDOM is STM32VL capable to read microseconds of TTL logic? I am trying to make it work on VL befor I burn my F4

xtian
Associate II
Posted on February 01, 2013 at 16:36

by the way I've tried this code in debug Mode... I am manually triggering the pins and it is working... wondering y it is not working in actual. though I have verified the signals in scope and in logic analyzer.

Posted on February 01, 2013 at 20:38

so there's nothing wrong with my GPIO code? its fully optimized?

Can't say I know enough about the solution to have an opinion.

If timing is critical, I'd latch the data externally, and then toggle a pin, or generate an EXTI interrupt.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
xtian
Associate II
Posted on February 06, 2013 at 00:28

Hi Clive... thank you very much... I have used STM32VL EXTI but it came out that it still lacks the speed that i need.. I would try my f4 now:) thanks!