STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use STM32F030F4

Posted on November 24, 2013 at 12:25Hello guys?      I have bought some STM32F030F4 chips ?but i donnot know how to program on it?I am confused of the Related firmware?So can someone tell me how to creat a new project using Keil-MDK without the give...

SPI MISO problem

Posted on November 23, 2013 at 23:09I know this is weird, but any help would be great. This is driving me nuts. I'm tyring to use A5, A6 and A7 as SPI for communication with a touchscreen controller. SCLK and MOSI work fine, but MISO (A6) works only...

SDIO clock doesn't seem to enable

Posted on November 22, 2013 at 17:19Hello community, I am trying to communicate a STM32F207 uC with a uSD card via the SDIO interface, what I am trying to do is to get the CID of the inserted uSD using CMD commands, and verify that both parts are co...

dmg0048 by Associate II
  • 1748 Views
  • 2 replies
  • 0 kudos

DCMI and DMA interrupts with phenomena

Posted on November 23, 2013 at 18:50 I'm now trying to receive an image from my OV9655 over the DCMI port and send it then to the pc. With low resolution (160x120 pixel) and saving the image in the ram it worked good. Now I want to geht higher r...

pa by Associate II
  • 2060 Views
  • 4 replies
  • 0 kudos

STM32 Interface with FSMC and DMA

Posted on March 21, 2012 at 12:56Hi, I have to read a 15 bit parallel data coming from a camera sensor and one bit as a request signal which tells whether the micrcontroller should initiate memory transfer or not. Does FSMC has any trigger signal ...

STM 32 F4 Discovery I2C Hanging Up

Posted on November 21, 2013 at 15:51Hi, I am having a problem with using the I2C on the STM 32 F4 discovery to read 3 DevanTech SRF-08 ultrasonic sensors, There was a previous post on this matter, but it was unresolved as far as I know, clive1 did i...

STM32f051C6 PF6/7 AF for I2C

Posted on February 26, 2013 at 07:38Hello, I try to make I2C on PF6/7 on the STM32F051C6  (48 Pin device) working. To get what AF to use, Ref man points to the datasheet. But the datasheet is not clear to me, it has a AF Table for PortA and PortB an...

jgnoss by Associate III
  • 3529 Views
  • 5 replies
  • 0 kudos

SPI DMA data corruption

Posted on November 21, 2013 at 17:52Hi,I am using SPI2 with DMA1 on STM32F427 to communicate with an external processor. The problem is that when the data on MISO and MOSI pins (PB14 and PB15) are somehow corrupted i.e. the data comes out as shifted...

asecen89 by Associate II
  • 2062 Views
  • 4 replies
  • 0 kudos

STM32F373 SDADC Gain Error Issue

Posted on October 23, 2013 at 21:20Using the 3 channels of the SDADC in Single Ended Zero Reference Mode, Gain 1, with a SDREF at 2.5V.  Spec lists gain error of -2.4% to -3.1%, but our devices appear to have a positive gain error of approx +2.8%.  ...