STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Label Verification

Hello, I have recently received a shipment of STM32F446RCT6 microcontrollers and I need verification of the ST label for quality assurance and production clearance. Could you please assist in confirming if the attached label and packaging details con...

Louay7 by Associate
  • 71 Views
  • 1 replies
  • 1 kudos

external memory selection for STM32H745 ?

Hi Team,I am working on board design using STM32H745 (LQFP176 package), and I would like to confirm the correct external memory selection for my smart kitchen application.Application details:- MCU: STM32H745 (dual core)- Package: LQFP176- USB OTG FS ...

STM32G0C1 USB 2.0 Type-C connection issue

Hi everyone,I have successfully implemented a USB VCP device on STM32G0C1 microcontroller, and it communicates perfectly with my PC.To meet current product trends, I am migrating the connector to USB Type-C (schematic attached). I am keeping it as a ...

Dillon_TUNG_1-1779074115220.png

Data Flash FLASH_EDATAxR_PRG Register Documentation

Hello,   In the reference manual rm0481 (stm32h562) in chapters 7.11.38 and 7.11.51 it is stated that EDATAx_STRT Bits do not have any hardware effect. Can I assume that the corresponding bits in FLASH_EDATAxR_CUR are set from option bits only? In th...

Nabidev by Associate II
  • 159 Views
  • 2 replies
  • 0 kudos

Address swapping of SDRAM

Hi ST Community, I am working on STM32H563 with external SDRAM connected through FMC. I am trying to use: heap in SDRAMglobal variables in SDRAMexecution/data access from SDRAMDCACHE enabled Current SDRAM mapping: 0xC0000000 I noticed that in STM32F7...

C5: Is BL_COM_CFG documented?

C5  implements a way to de-activate selected boot devices. This will allow to use the system bootloader on custom board were some activity on pins used by the bootloader but not used for the bootloader would inhibit use of the bootloader. This featur...

STM32H533CET6/STM32H533CET7 COUNTRY OF ORIGIN ISSUE

Dear Team,           Currently we are seeing part below in stock, Can we know if the parts were also assembled in China. Can you please check and confirm on the same. We are planning to procure 250# for production purpose.  MPN: STM32H533CET6 (or) ST...

STM32H523 Non-chinese origin

Dear Team,       We are currently using STM32H523CET6 in our designs. Can you please let us know if there any one is to one non- chinese alternative for the same. Please provide your support on this by treating this as critical, because we are holdin...

Resolved! STM32H523 MCU unwanted dependency between PB14 and PC9 pins

 Hi everyone,I am working on an STM32H523 MCU and I have recently observed some strange behavior regarding the PB14 and PC9 pins. I have the following setup:PB14 is configured as input (I use this for the TIM2_CH2 alternate function, but this does no...

rbnt by Associate
  • 698 Views
  • 2 replies
  • 4 kudos