2025-07-21 7:28 AM
Hello,
I'm working with the STM32H723 and need to interface with an external ADC that provides a DRDY (PG2 pin) signal. I'd like to initiate an SPI transfer via DMA whenever the DRDY pin goes low. The ADC is connected to SPI6, and I understand that only BDMA can be used with this peripheral.
My main question is:
How can I configure DMAMUX to trigger a BDMA transfer for SPI6 when the DRDY pin goes low?
I'm using STM32CubeMX for configuration. I’ve looked through existing forum posts and the STM documentation, but haven’t found a clear example or explanation for this setup. Any guidance, examples, or tips to get started would be greatly appreciated.
Thanks in advance!
2025-07-21 8:51 AM
According to DMAMUX2 and BDMA connections table in RM0468, exti_syscfg_exti2 is an input to the DMAMUX generator, as dmamux2_gen21, so this should be doable by selecting PG2 in the EXTI2 selector in SYSCFG and setting up DMA generation in DMAMUX2. I don't use Cube, so can't help with that; but I'd assume there's some clicking related to these facts in CubeMX. Maybe somebody versed in CubeMX will chime in with the details.
I presume you already know how to set up SPI with DMA - I do not know that, SPI in 'H7 is an overcomplicated beast and I don't use the 'H7.
JW
2025-07-22 1:51 AM
/* Local variables */
HAL_DMA_MuxRequestGeneratorConfigTypeDef pRequestGeneratorConfig = { 0 };
/* DMA controller clock enable */
__HAL_RCC_BDMA_CLK_ENABLE();
/* Configure DMA request hdma_bdma_generator0 on BDMA_Channel1 */
hdma_bdma_generator0.Instance = BDMA_Channel1;
hdma_bdma_generator0.Init.Request = BDMA_REQUEST_GENERATOR0;
hdma_bdma_generator0.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_bdma_generator0.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_bdma_generator0.Init.MemInc = DMA_MINC_ENABLE;
hdma_bdma_generator0.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_bdma_generator0.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_bdma_generator0.Init.Mode = DMA_NORMAL;
hdma_bdma_generator0.Init.Priority = DMA_PRIORITY_LOW;
if (HAL_DMA_Init(&hdma_bdma_generator0) != HAL_OK) {
Error_Handler();
}
/* Configure the DMAMUX request generator for the selected BDMA channel */
pRequestGeneratorConfig.SignalID = HAL_DMAMUX2_REQ_GEN_EXTI2;
pRequestGeneratorConfig.Polarity = HAL_DMAMUX_REQ_GEN_FALLING;
pRequestGeneratorConfig.RequestNumber = 1;
if (HAL_DMAEx_ConfigMuxRequestGenerator(&hdma_bdma_generator0,
&pRequestGeneratorConfig) != HAL_OK) {
Error_Handler();
}
hdma_spi6_tx.Instance = BDMA_Channel0;
hdma_spi6_tx.Init.Request = BDMA_REQUEST_SPI6_TX;
hdma_spi6_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi6_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi6_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi6_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi6_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi6_tx.Init.Mode = DMA_NORMAL;
hdma_spi6_tx.Init.Priority = DMA_PRIORITY_HIGH;
HAL_DMA_Init(&hdma_spi6_tx);
__HAL_LINKDMA(&hspi6, hdmatx, hdma_spi6_tx);
MX_SPI6_Init();
HAL_DMAEx_EnableMuxRequestGenerator(&hdma_bdma_generator0);
HAL_SPI_Transmit_DMA(&hspi6, dmaBuffer, 10);2025-07-22 2:16 AM
I don't use Cube/HAL, but I'd guess here
pRequestGeneratorConfig.RequestNumber = 1;
you have to set 10.
JW
2025-07-22 3:24 AM
Unfortunately, it did not work. Only 8 bits were transferred.
2025-07-22 5:04 AM - edited 2025-07-22 5:07 AM
Read out and check/post content of relevant DMA and DMAMUX registers.
> hdma_bdma_generator0.Instance = BDMA_Channel1;
> hdma_spi6_tx.Instance = BDMA_Channel0;
As I've said, I don't use Cube, but how do these things add up?
JW