STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F405 - measure two frequencies >= 10MHz

Posted on January 27, 2014 at 11:46Hey at all, First of all I want to say that my english isn't the best. I have got a new project to do it on a STM32F405 controller. I must measure two frequencies: 1. f1 = 13 to 16MHz 2. f2 = 10 to 13MHz my plan to...

EVALST7590T-2

Posted on February 10, 2014 at 16:27hi, i have 3 EVALST7590T-2, I would like to know if the boards are set as the default service node or as a base node and how to do and where to get the files to set them as a base node or service node. Thank you ...

STM32F Standby PowerManagement

Posted on February 09, 2014 at 16:40Hi, in my project a 2.8V voltage regulator is connected to the VDD pins of the STM32Fxx device. VBat is directly connected to a 3V battery. After reset the mcu processes some tasks and after that the controller f...

Trouble reading SD Card SCR Register with SDIO Peripheral

Posted on February 01, 2013 at 16:03I'm trying to read the SD CARD Configuration Register (SCR) on an SD memory card using the SDIO peripheral and I'm not sure if I'm approaching this in the right way, so I'm hoping someone here may have some experi...

dohzer by Associate II
  • 2212 Views
  • 2 replies
  • 0 kudos

SPI Clock via DMA

Posted on February 07, 2014 at 00:02I'm using a DMA for the first time (on a STM32F427), and am having a bit of trouble: I don't see SCK on any of my four SPIs when trying to transfer data via the DMA (specifically, I've only tried on the Tx side so...

jvavra by Associate III
  • 3604 Views
  • 13 replies
  • 0 kudos

STM32F4 Discovery ADC

Posted on February 07, 2014 at 10:46The original post was too long to process during our migration. Please click on the attachment to read the original post.

tiche79 by Associate II
  • 3360 Views
  • 9 replies
  • 0 kudos

.NET Micro Framework in STM32F429 Discovery Board

Posted on February 07, 2014 at 11:15DearI saw STM32F429 discovery board is MF supported. And I looked up the all functions, and it is not include Ethernet. But, only binary image files are offered on the web site. Is there any way of getting porting...

jwoh by Associate
  • 1357 Views
  • 2 replies
  • 0 kudos

STM32F103RG

Posted on January 29, 2014 at 10:33hallo, to program the STM32 microcontroller of my EVALST7590T-2 as base node or service node i can use the STMLINK and if i must to connect on STM32 UART SERVICE or on STM32 SWD ? And then what must i do? thanks. S...

Two USARTs

Posted on February 07, 2014 at 15:23Hi,I am trying to use two USARTs at the same time, but I can't get it to work.First:void RCC_Configuration(void){  /* USART1 clock enable */  RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);  /* USART2 clock...

nygaard by Associate II
  • 1260 Views
  • 2 replies
  • 0 kudos

STM32F429 Disco not running at 180 MHz, but 56 MHz

Posted on February 08, 2014 at 05:25 Could somebody help me to determine why my board is running at third of the speed. I am using emBlocks IDE and STM32F429I-Discovery_FW_V1.0.1 library. The loader code calls SystemInit (row 337 in system_stm32...

0690X00000603H9QAI.jpg 0690X00000603HAQAY.jpg
olavi by Associate III
  • 6729 Views
  • 8 replies
  • 0 kudos