User Activity

Posted on August 12, 2015 at 20:09Hi,I am using STM32F407 with uvision4, RL-TCPnet from keil and I have a problem in the Ethernet inicialization.When I turn on the PC and turn on the board at the same time the Ethernet doesn’t work, but if I turn on...
Posted on May 15, 2014 at 17:06 Hi,  I am using uvision4 with stm32f1xx to meansure frequency counting the time of the falling edge pulse. I need a high precision to meansure frequency from 0Hz to 240Hz. The first thing that I do was to set the pre...
Posted on September 25, 2013 at 13:53 Hi, I am using the DSP Library to make a Fir Filter with STM32F407 and uvision4. The example work fine and the data is right comparing with matlab. Now I am trying to make it work in a real time app...
Posted on July 25, 2013 at 19:17Hi all,I am using the STM32F207IG with uVision4 from Keil.For my suprise, the perfomance analyzer didnt apear in the Debug Section.I have found this link that show how to active: ''http://www.keil.com/support/man/docs...
Posted on July 05, 2013 at 15:12Hi,I didnt find nothing in the datasheet refering the data update rate of the calculations that STPM01 do. Do any one knows? I gues that it is 16,66ms but I am no sure.Bye