cancel
Showing results for 
Search instead for 
Did you mean: 

Flashing form windows command line

berge472
Associate II
Posted on May 16, 2013 at 18:53

I have a project where I will need to flash a few hundred chips that are already on boards. I have set up a chain programmer which is controlled by an MCU. basically it is just a chain of sockets for the boards that all get connected to an st-link v2, and it sequentially powers up the boards and runs a bat file to flash them. But I cant seem to find any information on using the st-link utility in windows command line. I use it linux, but this project will be used by our assembly department and they all run windows 7.

Does anyone have any information on using the st-flash in command line on windows?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on June 05, 2013 at 11:41

Hello,

You can use the ST-LINK Utility command line interface (CLI).

See

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/CD00262073.pdf

 for more details on how to do it.

Regards,

ST.MCU

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.