STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Difference ST-LINK/V2 vs iar I-jet

Posted on February 26, 2014 at 15:39Hi, Which are the differences between ''ST-LINK/V2'' and ''iar I-jet'' over that ''iar I-jet'' power consumption can be measured. (this is the only difference?)

ADC help needed

Posted on February 25, 2014 at 11:44 Hi, I think I'm missing out something simple or doing something stupid. I'm trying to do adc conversion on 3 channels on ADC1 continuously (loop). I use EOC interrupt and store the adc value in buffer. ...

jonfs2000 by Associate II
  • 2276 Views
  • 5 replies
  • 0 kudos

dead-time insertion for only one channel

Posted on February 23, 2014 at 19:14Hello,I use TIM1 to generate a clock-signal at the gpio-output-pin TIM1_CH1. This signal will be generated until a rising edge is detected at TIM_ETR (gpio-input). So the output-signal will be immediately pulled d...

Tim 3 Clock Frequency Understanding

Posted on February 26, 2014 at 07:03 Hi i am referring to an example from the stm32f4 library. In the comment section : TIM3 Configuration: Output Compare Toggle Mode: In this example TIM3 input clock (TIM3CLK) is set to 2 * APB1 c...

(sd)Disk explore

Posted on February 25, 2014 at 18:16Hi,  I am trying to modify function static uint8_t Explore_Disk (char* path , uint8_t recu_level); from USB host example for writing our more than 1 subdirectory and for SD card. I added :             else if(recu...

jspika by Associate II
  • 1139 Views
  • 2 replies
  • 0 kudos

Dma1 Stream6 Uart 2 tx Fifo error

Posted on February 25, 2014 at 04:02 I use the dma to TX only, the rx is handled in a interrupt with no dma. I've been working on this for quite some time now and I Always get a FEIF6 interrupt. Specifically I get TC, HT and FE. I dont h...

STM32F051 KEIL RTX CMSIS Interrupt Handling

Posted on February 25, 2014 at 16:48Hi All, I am new on this forum and as well new to STM32 microcontrollers - almost two months working with them - so please be understanding if I will write something stupid or ask about something obvious. Thanks. ...

damian by Associate II
  • 1314 Views
  • 2 replies
  • 0 kudos

Help with STM32F4 Clock config

Posted on February 25, 2014 at 15:30 Hi guys, I need help to configure the stm32f4 clock to disable the pll and just work with the 8MHz external crystal of the discovery board. The goal is to reduce as much as possible the consumpt...

STM32f-4 Motor control - PWM not generate

Posted on January 16, 2013 at 11:39Hi, i'm using the stm3240f board with a stm32f4-series.I try to generate PWM but nothing happen.what i did : /*declaration-----------------------------------------*/TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;TI...