STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 LCD Max resolution issue

Posted on February 28, 2014 at 06:08Hello,I have a question for STM32F429 LCD support.I will try use the stm32f429 and lvds ic to controll the TFT-LCD(1024x768, LVDS).According to the STM32F42x STM32F43x datasheet, LCDC Supports up to SVGA(800x600) ...

abby21 by Associate
  • 750 Views
  • 0 replies
  • 0 kudos

STM32F103 USART DMA issue

Posted on February 26, 2014 at 15:29Hi all,I have a problem using the DMA with USART3 on an STM32F103 MCU:I've configured the USART3 to transmit a buffer (fixed length) one shot using the DMA (just transmitting, not receiving) and then stop transmit...

Flash Loader - no target to select

Posted on December 01, 2013 at 22:57I am able to connect to my STM32F427 processor via FLD, but there is empty list, where you select target. I also get info about PID: 0419; BID: NA; Version 3.1.If I click next, and want to upload a file, it says t...

jernej by Associate
  • 2441 Views
  • 4 replies
  • 0 kudos

problem with FreeRTOS and USB

Posted on February 26, 2014 at 16:37hello everyone today I have a problem but I don't have any solution for that my problem: with USB per 1(ms) send 1 interrupt to system and if not solve this interrupt, the data will be broken                      ...

STM32F103 - Trying to measure Duty Cycle on 20Khz signal

Posted on February 21, 2014 at 23:16 Hello, I am trying to use a STM32F103 (8Mhz external clock) to get the duty cycle of a 20 Khz PWM signal. I am using Timer2 and trying to look at the rising edge using channel 1 and pointing channel 2 at ...

dirk23 by Associate II
  • 3464 Views
  • 5 replies
  • 0 kudos

STLink V2 on STM32F4 Discovery

Posted on February 26, 2014 at 11:17Hello,I have a STM32F4 Discovery. It has an on-board STLink V2 debugger that programs/debug the STM32F407 micro. I'm develloping a circuit that has also a STM32 micro and I would like to know if  I can use the STL...

Flash Loader Demo unable to erase stm32f207vg

Posted on February 26, 2014 at 11:08When i use the flash demo to erase my mcu, i selected erase all and click Next, flash demo tell me ''FAIL: Unable to erase flash''.What's wrong? Where can I get more information about it?thanks.   

0690X00000602rLQAQ.jpg

Difference ST-LINK/V2 vs iar I-jet

Posted on February 26, 2014 at 15:39Hi, Which are the differences between ''ST-LINK/V2'' and ''iar I-jet'' over that ''iar I-jet'' power consumption can be measured. (this is the only difference?)