User Activity

Posted on May 29, 2014 at 16:56hi, i am using stm32f103ret6 to test the voltage from the signal genarator(DG1022 from rigol). i found the adc of stm32 is nonlinearity. i found that,when the voltage from DG1022 is less than 1V,the voltage get from ad...
Posted on July 08, 2013 at 05:06stmstudio can't display static variable ?? #stmstudio #stm32
Posted on July 04, 2013 at 15:04Can i debug stm32 with stm-studio and MDK together? I found that stm-studio and MDK can not debug stm32 at the same time. The reason is ST-LINK(v2) can not be connected by MDK and STMStudio at the same time.  #stm3...
Posted on May 29, 2013 at 12:42can i trigger sdadc1 with  OC2 of tim19 ,and trigger sdadc2 with OC3 of tim19? then sdadc1 trigger dma2 in channel3,sdadc2 trigger dma2 in channel4.can stm32f373 do this ?? #stm32f373